For Immediate Release
Contact: mktgcomm@tams.com
TUSTIN, California — May 20, 2009 — Toshiba America Medical Systems, Inc. today introduces two advanced multi-detector CT systems, the Aquilion® Premium edition and the Aquilion CX edition. The Aquilion Premium rounds out the company’s CT portfolio to include a product with 160-detector rows and coverage up to 8 cm in a single rotation. This system is also field-upgradeable to an Aquilion ONE. The Aquilion CX is Toshiba’s next generation 64-detector row CT system featuring faster reconstruction standards with up to 28 images per second, Toshiba’s proven Quantum Advantage detector technology and a patient couch that can accommodate up to 660 lbs. The Aquilion Premium and Aquilion CX are both available now.
“Toshiba is committed to listening to its customers and providing the right technology mix for the community,” said Doug Ryan, senior director, CT Business Unit, Toshiba. “We developed the Aquilion Premium and Aquilion CX to meet our customers’ ever-changing medical imaging needs. The Aquilion Premium provides an upgrade path to the Aquilion ONE, the world’s first dynamic volume CT, while the Aquilion CX is an advanced 64-detector row CT system that incorporates superior features of the existing Aquilion 64.”
Because the Aquilion Premium is field-upgradeable to an Aquilion ONE, this product enables the medical community to have access to advanced technology today, while allowing physicians and administrators to plan for their future needs. Additionally, the Aquilion Premium comes standard with the 72 kW generator, a 660 lb patient weight couch and advanced features like iStation display and 8 cm dynamic scanning capability.
Toshiba’s next generation 64-detector system, the Aquilion CX, is positioned as a comprehensive workhorse CT system and comes standard with faster reconstruction times of 28 images per second, the quickest in the industry. The Aquilion CX is designed for advanced, emergency and routine radiology exams and allows customers to image patients ranging from pediatric to bariatric. The CX features a 72 kW generator for wider mA scanning flexibility, coneXact® software for higher definition images for extremities and IACs, SUREExposure™ including QDS and Boost3D™ and double the console storage capacity of a conventional 64-detector CT.
The Aquilion CT product line has received numerous accolades including the number one ranking in CT from MD Buyline since 2002 (six consecutive years). The Aquilion CT line has also been named Best in KLAS in 2006 and 2007; Best in KLAS in 2008 for 64-detector row and above; and Frost & Sullivan’s “Healthcare Innovation Award in Cardiovascular Imaging” in 2008. (For more information about KLAS, visit www.KLASresearch.com.) Most recently, Toshiba’s service for the Aquilion line was ranked number one in 21 out of 34 ServiceTrak Imaging’s 2008 report on CT system service.
With headquarters in Tustin, Calif., Toshiba America Medical Systems markets, sells, distributes and services diagnostic imaging systems, and coordinates clinical diagnostic imaging research for all modalities in the United States. Toshiba Medical Systems Corp., an independent group company of Toshiba Corp., is a global leading provider of diagnostic medical imaging systems and comprehensive medical solutions, such as CT, Cath & EP Labs, X-ray, Ultrasound, MRI and information systems. Toshiba Corp. is a leader in information and communications systems, electronic components, consumer products, and power systems. Toshiba has approximately 198,000 employees worldwide and annual sales of $77 billion. For more information, visit www.medical.toshiba.com.
*Aquilion, Aquilion ONE and coneXact are registered trademarks of Toshiba Medical Systems Corporation.
*Boost3D and SUREExposure is a trademark of Toshiba Medical Systems Corporation.