Toshiba America Medical Systems | Leading Innovation

For Immediate Release
Contact: mktgcomm@tams.com

HARVARD TEACHING HOSPITAL BETH ISRAEL DEACONESS INSTALLS MOST ADVANCED CT SYSTEM AVAILABLE — Aquilion ONE DYNAMIC VOLUME CT

Toshiba’s Dynamic Volume CT Provides Faster, More Accurate Diagnosis While Lowering Healthcare Costs

BOSTON — May 20, 2008 — As a testament to the growing demand to improve patient care while reducing healthcare costs, Toshiba America Medical Systems, Inc. has installed the Aquilion ONE™ dynamic volume CT system at Beth Israel Deaconess Medical Center, a teaching hospital of Harvard Medical School in Boston.

“In one of the country’s leading medical teaching hospitals, we hope the Aquilion ONE’s ability to image an entire organ and show function for the first time will mean faster, more accurate diagnosis, better patient outcomes and ultimately lower healthcare costs for our patients,” explained Dr. Vassilios D. Raptopoulos, interim radiologist-in-chief, Department of Radiology and director, CT services, Beth Israel Deaconess Medical Center. “We are grateful to be one of the first teaching hospitals in the United States using this advanced technology.”

Toshiba’s Aquilion ONE dynamic volume CT system utilizes 320 ultra-high resolution detector rows (0.5 mm in width) to image an entire organ in a single gantry rotation. The result is unparalleled in diagnostic imaging today and produces a 4D clinical video showing up to 16 cm of anatomical coverage, enough to capture the entire brain or heart, and show its movement such as blood flow.

“The Aquilion ONE has the potential to provide a single, comprehensive exam that can replace a variety of duplicative and invasive procedures,” added Dr. Raptopoulos. “Its versatility and ability to diagnose disease fast will be used within our radiology department to detect and treat life-threatening conditions, including cancer, heart disease, stroke and other neurovascular conditions.”

“Toshiba designed the Aquilion ONE for today’s healthcare environment,” said Doug Ryan, senior director, CT Business Unit, Toshiba. “By replacing several tests with this single exam, the Aquilion ONE will allow physicians to treat at-risk patients immediately — saving resources and time for both healthcare facilities and patients.”

About Beth Israel Deaconess Medical Center
Beth Israel Deaconess Medical Center is a patient care, teaching and research affiliate of Harvard Medical School, and consistently ranks among the top four in National Institutes of Health funding among independent hospitals nationwide. BIDMC is clinically affiliated with the Joslin Diabetes Center and is a research partner of Dana-Farber/Harvard Cancer Center. BIDMC is the official hospital of the Boston Red Sox. For more information, visitwww.bidmc.harvard.edu.

About Toshiba
With headquarters in Tustin, Calif., Toshiba America Medical Systems markets, sells, distributes and services diagnostic imaging systems, and coordinates clinical diagnostic imaging research for all modalities in the United States. Toshiba Medical Systems Corp., an independent group company of Toshiba Corp., is a global leading provider of diagnostic medical imaging systems and comprehensive medical solutions, such as CT, Cath & EP Labs, X-ray, Ultrasound, MRI and information systems. Toshiba Corp. is a leader in information and communications systems, electronic components, consumer products, and power systems. Toshiba has approximately 191,000 employees worldwide and annual sales of $67 billion. For more information, visit www.medical.toshiba.com.

 
 

Terms & Conditions | Privacy Policy © 2012 Toshiba Corporation