Toshiba America Medical Systems | Leading Innovation

For Immediate Release
Contact: mktgcomm@tams.com

TOSHIBA DEMONSTRATES NEWEST CT SOFTWARE AT ACC

Recently Cleared by the FDA, SURECardio Prospective and Variable Helical Pitch Will Improve Patient Care and Workflow While Reducing Dose

CHICAGO — April 1, 2008 — Toshiba America Medical Systems, Inc. is committed to new CT clinical applications that improve throughput and workflow, while further reducing contrast and radiation dose to patients. At this year’s American College of Cardiology annual meeting in Chicago, March 30 – April 1, 2008 (Booth # 8001), Toshiba will demonstrate new applications that embody this commitment — SURECardio™ Prospective and Variable Helical Pitch (vHP), which was recently cleared by the FDA.

SURECardio Prospective
Toshiba’s SURECardio Prospective helps reduce patient dose by up to 80 percent during coronary CTA exams by using a helical acquisition technique to provide one continuous image instead of multiple images produced by the current step-and-shoot techniques.SURECardio Prospective will automatically detect and adjust to patients with irregular heartbeats, providing quicker, more conclusive exam results.

SURECardio Prospective automates scan parameters and reconstruction based on the patient’s heart rate. It also speeds exam time and eliminates the requirement for additional contrast used with the step-and-shoot method.

Variable Helical Pitch
Variable Helical Pitch (vHP) increases workflow and efficiency by enabling physicians to complete an exam of more than one anatomical region consecutively – i.e. without stopping to alter the helical pitch of the exam. This gives physicians the flexibility needed for cardiovascular imaging. For example, patients with suspected chest pain can now undergo one CT exam to detect both heart disease and an aortic aneurysm.

Toshiba is the first vendor to clinically introduce this type of technique.

“Previously, if a physician needed to image a patient’s heart and aorta, either one higher dose or two separate exams would have been needed,” explained Doug Ryan, senior director, CT Business Unit, Toshiba America Medical Systems. “vHP reduces both patient radiation and contrast dose and also saves time because both regions can be scanned with one exam. This technique is a prime example of how Toshiba is innovating its technology to help patients and physicians.”

vHP also saves time by producing one comprehensive image instead of two separate images that would result from separate scans. This eliminates the task of piecing together separate images.

Both clinical applications are available to purchase independently and will be offered with all new AquilionTM 32 and 64 CT systems.

About Toshiba
With headquarters in Tustin, Calif., Toshiba America Medical Systems markets, sells, distributes and services diagnostic imaging systems, and coordinates clinical diagnostic imaging research for all modalities in the United States. Toshiba Medical Systems Corp., an independent group company of Toshiba Corp., is a global leading provider of diagnostic medical imaging systems and comprehensive medical solutions, such as CT, Cath & EP Labs, X-ray, Ultrasound, Nuclear Medicine, MRI and information systems. Toshiba Corp. is a leader in information and communications systems, electronic components, consumer products, and power systems. Toshiba has approximately 191,000 employees worldwide and annual sales of $60 billion. For more information, visit www.medical.toshiba.com.

SURECardio and Aquilion are trademarks of Toshiba Medical Systems Corporation.

 
 

Terms & Conditions | Privacy Policy © 2012 Toshiba Corporation