Toshiba’s Infinix-i Cardiovascular X-ray Helps Make Interventional Procedures Safer for Patients with the Transradial Approach
October 13, 2011
Using the radial artery to perform cardiac catheterizations is proven to lower the risk of vascular complications, reduce major bleeding and improve patient recovery time when compared to femoral access. The number of cardiac catheterizations in the U.S. done using the radial approach, currently 8 percent, is rapidly growing¹ as healthcare facilities realize the patient benefits. With a commitment from physicians and the right imaging technology, successfully using the radial approach is possible. One example is Shannon Medical Center, in San Angelo, Texas.
In the past few years, Shannon Medical Center, a 250-bed community hospital, focused on making the radial artery the access point of choice, which resulted in improved safety and outcomes for patients. Shannon Medical Center needed a new vascular X-ray imaging system to accommodate the right or left side radial approach and that was flexible enough to perform various cardiac interventional and other procedures.
Dr. J. Chris McClish, interventional cardiologist at Shannon Medical Center, led the search for the new imaging system and selected Toshiba America Medical Systems, Inc.’s Infinix™ VF-i single plane vascular X-ray system.
“Radial artery access is undeniably the future of cardiac catheterization and the flexibility and image quality of the Toshiba Infinix-i system allows safer, more efficient interventions,” said Dr. McClish. “For example, the system’s lateral movement and fingertip-to-fingertip coverage enable catheter exchanges during procedures without adjusting the table and changing alignment. As our default access site, radial reduces complications and improves patient satisfaction.”
The Infinix VF-i single plane is a dedicated cardiac cath lab featuring a floor mounted five-axis positioner, making it possible to obtain images without re-positioning patients. This allows clinicians unencumbered patient access and an ergonomic set-up, along with the ability to maneuver over the heart and down to the wrist. The Infinix-i monitors also float freely around the system and can be positioned for easy viewing regardless of right or left side radial approach.
Shannon Medical Center’s Radial Results
Within months, the Infinix VF-i system helped Shannon Medical Center increase radial procedure volume to approximately 65 percent of the 1,600 catheterization cases done per year, well above the national average. Shannon’s ability to perform this procedure with minimal complications and increased patient satisfaction has created a competitive advantage for the hospital, with patients traveling from all over the region for treatment.
With Toshiba’s Infinix-i X-ray system and a dedicated commitment from the hospital, transradial interventions can be done more frequently for safer exams that drive patient satisfaction and can provide competitive advantage for hospitals.
¹“Wrist May Be Route to Safer Heart Treatment,” Wall Street Journal, February 8, 2011.