Improving Utilization With Shared Laboratories
June 28, 2010

As hospitals continue to want to improve utilization of imaging equipment, many are turning to a new solution: shared cardiac/vascular-catheterization laboratories. “It’s going to become increasingly important for hospitals to find imaging systems that are versatile and can meet all of their imaging needs” Allan Berthe, Toshiba’s senior cardiology product manager, explains.
Berthe says that smaller flat-panel detectors are ideal for imaging the heart, but a larger detector is required to cover a larger anatomical area. Toshiba’s dual-plane Infinix DP-i system solves this problem by incorporating two C-arms and two flat-panel detectors on the same unit: a floor-mounted eight-inch panel and a ceiling-mounted 12×16-inch panel. “The two C-arms operate independently; one is dedicated to cardiac cases and the other is dedicated to vascular cases,” Berthe says. “You can quickly exchange those back and forth in less than 60 seconds—a capability no other system in the industry offers.”
Working with a shared system saves valuable hospital space and reduces both maintenance and staff costs, but the advantages don’t end there, Berthe notes. “The smaller flat-panel detector can easily image the heart, but it’s not uncommon for a patient with coronary-artery disease also to have problems elsewhere in the body,” he says. “If you want to perform two procedures on the same patient (looking at the heart and the legs, for example), the DP-i excels. You could use the small panel to look at the heart and then quickly change over to the large panel to look at both legs in one view.”
The Infinix-i DPi boasts multiple features aimed at bolstering its clinical flexibility, including a flexible C-arm for peripheral angiography, optional 3D angiography, a table that can accommodate patients weighing up to 484 pounds, and two liquid-metal–bearing X-ray tubes, one for cardiac work and one for full-body imaging. “The dual-plane systems allows you to do both types of imaging with a lot of freedom,” Berthe says. “The user will never have to compromise on the anatomy he or she wants to image.”