Login: Image Maker

ACC Preview: Advances in Cardiac Imaging

March 1, 2010

At this year’s annual scientific meeting of the American College of Cardiology (ACC), which takes place on March 14–16 in Atlanta, Toshiba (booth #1944) will showcase a range of advances in and enhancements to its cardiac-imaging technology.  Following is an overview of what Toshiba will showcase:

Infinix-i Hybrid Lab

When performing patient procedures in a hybrid setting, it is critical that the imaging system provides the flexibility to quickly and easily access both the patient and ancillary equipment. Toshiba will showcase its Infinix™ VF-i vascular X-ray system with 12” x 12” flat panel detectors and CAT-880B hybrid catheterization table, designed to create a best-in-class hybrid suite.  The new mid-sized 12” x 12″ flat panel detector expands the versatility of the Infinix-i line that features a five-axis C-arm positioner and enables unprecedented patient access and coverage. Along with the new mid-sized detector, the Infinix-i five-axis systems are now available with the new CAT 880B tilt/cradle hybrid catheterization table. This table is designed to allow greater positioning flexibility and patient access during imaging and surgery. The table functionality, with side-to-side cradle and head-to-toe tilt, permits clinicians to angle the table in the optimal position to quickly and comfortably complete procedures. The system on display will also include ancillary equipment typically used in a hybrid suite.

Cardiac Ultrasound Capabilities

The cardiac capabilities of Toshiba’s ultrasound technology will also be featured. The Aplio Artida™ system is a dedicated cardiac system which provides unique 3D Wall Motion Tracking, allowing physicians to rapidly identify wall-motion defects and the timing of cardiac events, as well as real-time, multiplanar reformatting for assessing global and regional left ventricular function. Also on display is the new Aplio™ MX system, which is midsized and cart-based for better portability. Aplio MX is a multi-modality system which includes Differential Tissue Harmonic Imaging, for better results with bariatric patients; ApliPure, which enhances image clarity and detail definition; Advanced Dynamic Flow, which shows flow with directional information for even the smallest vessels.

Cardiac CT Software Enhancements

CT will highlight cardiac-software enhancements for the Aquilion® ONE and Aquilion Premium, including new ONE Beat Prospective Reconstruction, which shortens the interval window and reduces radiation exposure time, reducing dose by 21 percent; Real Time Beat Control, which calculates the running real-time average of the heart rate to predict the next beat more precisely (and thus, to time the scan more accurately); and optimizing timing for SUREStart, which accurately determines contrast uptake time for a better image. Wide Volume Cardiac Protocol on the Aquilion ONE, a work-in-progress enhancement, will enable clinicians to image the entire heart, lungs, and aorta in two rotations.

Cardiac MR

The wide range of cardiac MR capabilities on the Vantage Titan™ and Vantage Atlas® systems will be highlighted. The Vantage MRI product line offers a range of advanced cardiac capabilities, including a cardiac coil for the Vantage Titan and noncontrast imaging for patients with renal insufficiency.

Click here to download a printer-friendly version.