TOSHIBA RECEIVES FDA CLEARANCE FOR VANTAGE ZGV MRI SYSTEM
MRI System Boasts Advanced Capabilities for Cardiac Imaging Applications
ACC Booth # 4119
ATLANTA, March 11, 2006 – Toshiba America Medical Systems, Inc.
(TAMS) today announced FDA clearance for its high performance Excelart VantageTM ZGV
magnetic resonance imaging (MRI) system, the most sophisticated 1.5T system in the
industry. The new Vantage ZGV is immediately available and offers new product
sequences, enhanced image quality, and features the Mach 8 processor, increasing
reconstruction to 1300 images per second for more powerful clinical applications.
“The ZGV continues
our tradition of creating high quality, innovative products that best serve patient
and clinician needs for advanced cardiac imaging applications,” said Bob Giegerich,
director, MR Business Unit, TAMS. “Featuring the reliability and accuracy
that have become trademarks of Toshiba’s line of Vantage products, the ZGV offers
even more sophisticated features to help improve diagnosis and overall patient comfort.”
The Vantage ZGV
offers a gradient strength of 33 mT/m (milliTesla per meter), a slew rate of 200
mT/m/ms (milliTesla per meter per millisecond) and delivers the highest homogeneity
of any magnet in the industry over the full 50 cm diameter spherical volume (DSV).
Field upgrade kits to the new ZGV are available to current Vantage users.
Vantage
MRI—Unmatched Performance and Patient-Focused Features
In addition to the ZGV model, the Vantage is available in three other versions offering
an ultra-short magnet at 140 cm with linear 30 mT/m gradient strength and a slew
rate of 50 mT/m/ms on the AGV, the 86 mT/m/ms on the MGV and 130 mT/m/ms on the
XGV.
Featuring some
of the most advanced MRI applications available in the industry, the Vantage includes
optional packages for cardiac imaging, advanced Echo Planar Imaging (EPI), Perfusion
and Diffusion Imaging, Peripheral MRA (magnetic resonance angiography), and SuperFASE
(Fast Advanced Spin Echo) imaging. In addition, Toshiba has pioneered research
into contrast-free MRA with its Fresh Blood Imaging (FBI) protocol and Body Diffusion.
With Toshiba's
patented PianissimoTM technology, which reduces acoustic
noise by as much as 90 percent, the Vantage dramatically reduces the most significant
cause of patient discomfort and enables clinicians to better utilize all of the
system's high-field MRI capabilities including SPEEDER parallel imaging for increased
acquisition speed and reduced examination times. For more information about
the Vantage, TAMS and its wide range of medical imaging products, visit
www.medical.toshiba.com.
About
Toshiba
With headquarters in Tustin, Calif., Toshiba America Medical Systems markets,
sells, distributes and services diagnostic imaging systems, and coordinates clinical
diagnostic imaging research for all modalities in the United States. Toshiba
Medical Systems Corporation, an independent group company of Toshiba Corporation,
is a global leading provider of diagnostic medical imaging systems and comprehensive
medical solutions, such as CT, X-ray, Ultrasound, Nuclear Medicine, MRI and information
systems. Toshiba Corporation is a leader in information and communications
systems, electronic components, consumer products, and power systems. Toshiba
has approximately 161,000 employees worldwide and annual sales of $53 billion.
Excelart VantageTM and PianissimoTM are
trademarks of Toshiba Medical Systems Corporation.